AXIS#.VL.FBSOURCE
Description
This parameter determines the feedback source to be used by the velocity loop.
| Value | Definition |
|---|---|
| 0 | Defers selection to AXIS#.IL.FBSOURCE - this is the default, and uses the value which is being used for commutation |
| 1 | Selects FB1 (connector X1) |
| 2 | Selects FB2 (connector X2) |
| 3 | Selects FB3 (connector X23) |
| 4 | Selects FB4 (connector X21) |
| 5 | Selects FB5 (connector X22) |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 5 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Related Topics
|
Copyright © 2018 Kollmorgen |
|